Other Parts Discussed in Thread: DRV8462, DRV8461
Hi, I'm using DRV8834 to control a stepper motor in indexer mode without any brake system on actuator.
so some amount of current should flow on coils to hold the position in idle state of the actuator.
but I concern about getting heat by the holding current because the idle time is quite long.
our system don't need high torque, so I think it is okay that half amount of current than in running state is enough in idle state.
could you share some methods to control the amount of current in idle state using indexer mode?
or any other methods to manage temperature?
thanks in advance.