Other Parts Discussed in Thread: MCF8329A
I have the following HW setup:
1. MCF8316AEVM
2. Maxon 449464 motor
3. 24V 3A bench power supply
Default registers preset loaded using Motor Studio and then MPET runs successfully with 60% default rated peak current, 6000RPM and 7 Pole Pairs configuration.
Next, I rotate the potentiometer counter-clockwise fully so the motor runs at 6000RPM loaded; PSU showing driver drawing about 1.4A.
Then I don't know what happens but the motor suddenly stops with no fault displayed in Motor Studio, this can happen anytime between 10 minutes and 1 hour, I haven't tried for longer run times.
When it stops, it can either go short (PSU hitting current limit and 24V dragged down) or it just stops in an idle condition (24V 40mA) unable to restart by turning the potentiometer (power cycle required).
No fault LEDs displayed on the evaluation board.