This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCF8316C-Q1: 150W Motor Driver Recommendation Request

Part Number: MCF8316C-Q1
Other Parts Discussed in Thread: MCF8329A, MCF8329A-Q1

Hi, 

My customer is reviewing 150W motor drivers.

Application : Car Electric Water Pump

Customers have two specifications.

1. BLDC Motor

- FOC ready Code-Free Smart Driver

- 150W (Operating Voltage : BATT 12V)

- Diagnostic functions: motor overcurrent, motor open circuit, motor short circuit, IC over temperature


2. DC Motor F/Bridge

- 150W (Operating Voltage : BATT 12V)

- Diagnostic functions: motor overcurrent, motor open circuit, motor short circuit, IC over temperature