This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8849: Driving a motor using a DRV8849.

Part Number: DRV8849

Tool/software:

Our application uses the DRV8849 driver to control motor rotation. However, we're encountering a motor noise issue during operation with a load of 0.4 Nm.
Could you please suggest optimal driver settings to reduce the noise?
Here are the current driver settings we are using:

  • Full step mode, without any microstepping. Our mechanical setup uses a 1:8 gear ratio, meaning 8 motor rotations result in 1 full rotation of the mechanical system.
  • The motor operates at 120 RPM to achieve a mechanical speed of 15 RPM due to the 1:8 gear ratio.

Your guidance would be greatly appreciated.

  • Hi Rohit,

    What was the decay mode setting used? Could you please share the current waveform for one of the windings? Typically stepper motors tend to have higher audible noise in full-step mode. Using microstepping and smart tune ripple control decay mode would significantly reduce the audible noise of the stepper motor.

    Regards, Murugavel