Hi Team,
The customer uses DRV8849 to drive a motor, and the OUT1A, OUT1B, OUT2A, and OUT2B outputs control a motor.

Raise the following pins:
ENABLE1, ENABLE2 ,
NSLEEP
STEP1 and STEP2
MODE01 and MODE11
VREF1 and VREF2
But the motor didn't rotate and kept getting hot. He used a multimeter to measure that the output was 5v.
How should he configure the pins of drv8849 to make the motor rotate?
Regards,
Annie