Other Parts Discussed in Thread: DRV2911, ULC1001
Tool/software:
Hello,
I am trying to build a test board using ULC1001 and DRV2911. Please review the attached schematic and layout.
0910_ULC1001_DRV2911_LAYOUT.pdf0910_ULC1001_DRV2911_CIRCUIT.pdf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello,
I am trying to build a test board using ULC1001 and DRV2911. Please review the attached schematic and layout.
0910_ULC1001_DRV2911_LAYOUT.pdf0910_ULC1001_DRV2911_CIRCUIT.pdf
Hi Wonbin,
Thanks for reaching out. We will review and provide the feedback as soon as possible in the next 1-3 business days.
Best,
Hailong
Hi Wobin,
I have been reviewing the schematic and the layout. How do you choose the LC filter values at the output after the DRV2911? Note that the LC filter values and some components are designed based on the specific load, which is the Lens Cover System.
Hello,
The LC filter values were selected to suit the characteristics of the self-made load.
Is it okay to proceed with the LAYOUT as in the attached file?
Some suggestions are listed in the ULC1001 data sheet regarding the layout. Please check and follow the guidelines below.
Place a 1uF 16V capacitor close to IOVDD pin 27.
• VSNS Amplifier
– Minimize and match the traces going to VSNS_P and VSNS_N. Shield these traces from any high voltage
signals.
– Match the trace length and parasitics from the load to resistor R1. Reference Section 6.1.
• ISNS Amplifier
– Minimize and match the traces going to ISNS_P and ISNS_N. Shield these traces from any high voltage
signals.
– Match the trace length and parasitics from the load to resistor R4. Reference Section 6.1.
• Isolate any high voltage signals that may occur when driving the LCS from the low-voltage plane of the
ULC1001. Inserting a trench between planes is recommended
Hello,
I Have Two Question.
Q1. Can I get the PCB file of the ULC1001-DRV2911 evaluation module? (ex. Altium file, PADS file)
Q2. The resonant frequency of the piezoelectric element I created is 31.7 kHz.
To increase the resonance effect, I set L: 22uH / C: 470nF. (The cutoff frequency value is 49.49 kHz). Are L,C appropriate values?
You can find the EVM design files on https://www.ti.com/tool/ULC1001-DRV2911EVM
Regarding Q2, do you know what is the resonant frequency of the piezo/lens system? The LC filter is determined by the resonant frequency and the impedance of the final system. If the resonant frequency of the system is close to 31.7kHz, then the LC filter you choose is a good estimate. It might require a tuning based on the impedance response but you can tentatively put it there.