Other Parts Discussed in Thread: DRV3255-Q1
Tool/software:
I would like to request sch review of DRV8353. Can you please get back to me? Thx!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
I would like to request sch review of DRV8353. Can you please get back to me? Thx!
Hi Leo!
Thank you for reaching out on our forum.
I would be happy to help with a schematic review - can you please upload here the DRV8353 schematic in PDF form?
Best Regards,
-Joshua
See attached. Please focus on p1 and 4 where the totem pole and DRV8353 are.
We had many failures in our current design with phase current of ~ 300A. Likely caused by the external voltage spike across SP and SN.
Thanks Leo!
I will look into the schematic information, so please look forward to the feedback by the end of Wednesday.
Regarding the CSA selection I am not currently familiar, and may recommend actually posting another E2E to receive guidance from the Instrumentation Amplifier product line engineers.
Best Regards,
-Joshua
Thank you!
My biggest worry is the integrated current sense opamp failing after reading a bunch of posts on TI's E2E.
Please note the abs max operating condition is 300A phase current for 2sec. I had parallel CSR (WSHP28181L000FEA) to support the pulse "overload" but I really want to make sure the RC element connected to the internal op-amp is properly tuned.
Hi Leo,
Of course! I understand the concern, however as long as the shunt resistor is sufficiently sized to reduce the voltage observed on the CSA input pins, there should be no issue as long as this high worst-case scenario is kept in mind during the design phase.
I am still overviewing the design but will follow-up within a day with my additional feedback.
Best Regards,
-Joshua
Hi Leo,
Thank you for the clarification and additional questions here.
Let me see if there may be a good INA recommendation for your application.
For the parallel FETs i would recommend MOSFETs with a much lower Qgd (>100nC).
For the datasheet and NDA request, please reach out over email or through another E2E thread with that request as the topic, since I am unable to provide that.
Best Regards,
-Joshua
Hi Leo,
Regarding the schematic design for the DRV8353, I believe it to be sufficient. However, I have one concern regarding the resistor on SNX (R203):
Is this resistor also 0-Ohm (like SPx R202) or is it 5.1ohm as designated in the schematic?
I would caution against having a valued resistor on only one of the sense lines, as that would affect the voltage differential on the internal sense amplifiers.
Best Regards,
-Joshua
My intent is to have symmetric RC filter applied to the CSA, however, DRV8353 does not differentiate between SPx and LS FET source connection thus R202 = 0ohm (ideally it should be 5 ohm).
I will probably make R202=5ohm and reduce LS gate resistor = 0 ohm.
Do you have a set of recommended values for IAUS300N10S5N015TATMA1 MOSFET?
This is our current setting.
Fsw: 20kHz
1% DT= 1/(20e3)/100/1e-6= 500nS
SPI reg setting
tDEAD=11b (500ns DT i.e. 1% of Fsw)
I_DRIVEP (mid pull up)
I_DRIVEP_HS or I_DRIVEP_LS=1000b (550mA)
I_DRIVEN
I_DRIVEN_HS=100b (1000mA) moderate pull down when LS turn on
I_DRIVEN_LS= 111b (2000mA) strong pull down when HS turn on
tDRIVE= 11b default setting. No change.
Hi Leo,
Thank you for the clarification, and would suggest the R202 resistor as you stated.
Regarding the chosen settings, my only recommendedation is for these FETs of a gate Qgd of 50nC. Typically a rise/fall times between 100-300nS is recommended, so I would recommend an IDRIVE gate current between 200-500mA for highside and lowside.
If these FETs are in parallel, then would increase the gate current appropriately to ensure the split current in the layout affects the FETs' rise and fall times.
Hope this information has been helpful.
Best Regards,
-Joshua
Josh,
Another question for you.
Can you help confirm the following calculation is correct for "single supply power dissipation" as mentioned in DRV8353 ds eqn 33-38 ?
Do you know why the ds assumes 3 FETs are switching at any given time (see attached)?
We run FOC + SVPWM modulation so 1 FET changes state from one vector to the next, nominally.
Calculation leads to Tj ~ 130C (150C as abs max).
See blow
In addition.
FET_num=2;
Qg=223; %IPTC012N08NM5ATMA1/IPTC011N08NM5ATMA1
Qg_tot=FET_num*Qg
Fsw=20e3;
Factor=1/100;
rise_time_ns=Factor*(1/Fsw)/1e-9
I=Qg_tot/rise_time_ns
With Idrive <1A the DRV8353 should be able to support 2 paralleled FETs.
Let me know if this is correct.
Hi Leo,
Your calculation for a specific cycle (two highside FETs on and one lowside FET off) appears fine. And I believe the DS is grouping the high side and lowsides together per entire commutation cycle, as the power loss will utilize all 6 FETs.
Regarding the use of parallel FETs, the DRV8353 gate current selection should be capable of driving. Please find this application brief that provides insight into important considerations for using parallel FETs in BLDC system: https://www.ti.com/lit/ab/slvaf39a/slvaf39a.pdf
The document is for another DRV device, but the same principles and guidelines apply.
Best Regards,
-Joshua
Joshua,
RE: "And I believe the DS is grouping the high side and lowsides together per entire commutation cycle,"
I'm not sure if I'd agree to the calculation even its per commutation cycle basis.
There are only 3 FETs on at any given vector of SVPWM i.e. the "x3" in eqn(33) is incorrect (unless the gate driver is consuming the same amount of current even when the FET is off).
Regardless of which vector the controller stays in there are 3 FETs that are not consuming gate driver current.
Is my understanding correct?
Hi Leo,
Please let me look into this a bit further over the Thanksgiving holiday to better explain this topic and follow-up at the start of next with further response.
Best Regards,
-Joshua
Hi Leo,
I look forward to our meeting tomorrow to discuss and close your open inquiries!
Best Regards,
-Joshua