This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8353: Missing Gate Drive PWM Signals

Part Number: DRV8353


Tool/software:

Dear TI Support Team,

I am working with the DRV8353RH gate driver and have configured the following settings:

  • Mode pin: Tied to GND with 0Ω (6x PWM mode, Figure 38, Page 40)
  • IDRIVE: Tied to DVDD (1/2 A, Figure 39, Page 40)
  • VDS: Tied to DVDD with 18kΩ (VDS = 1V, Figure 39, Page 40)
  • GAIN: Tied to GND (5V/V, Figure 38, Page 40)

Measured node voltages:

  • Vdvdd = 5.2V
  • Vin = 52.08V
  • Vm = 15.02V (Refer to Page 26 for details)

Issue:
Primary Side PWM signals are 16 kHz measured across all 6 channels and the Gate Drive Enable voltage as 3.3V (indicating that the gate driver should be active), but the secondary-side PWM gate drive signals are missing.

Could you help identify potential causes for this issue?

Thanks & Regards,
Himavanth Reddy