I'm wondering if anybody would be able to shed more light on how the DRV8412 handles it's cycle-by-cycle current limiting. The datasheet states that in CBC mode, current will be limited by the CBC but also protects the circuit with a latching shutdown. However, there is only 1 OC-adjust resistor. In CBC mode, is this resistor for the CBC limit or the latching shutdown limit? If anybody has delved into the current limiting of the DRV8412 and could shed some light on how it can be controlled, that would be greatly appreciated.
Regards,
Tyler