This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV3201-Q1 SPI

Other Parts Discussed in Thread: DRV3201-Q1

Hello,

I'm currently interested in the DRV3201-Q1 motor driver and was wondering, is possible to set speed through the SPI bus or  can it only be done through PWM? If it can't, then is SPI only really used for error detection and handling? Also, I know the EVM is only in preview right now, but is there any information on how much the MOSFETs can drive? And can PWM by supplied from an external MCU or something specific on the EVM? Thanks in advance.

Regards,

Jake

  • Hi Jake,

    1. SPI is only used for diagnosis, protection, and monitoring, not speed control.

    2. The DRV3201 does support PWM control (PWM Mode).

    3. The EVM supports up to 100A.

    4. The EVM has a connection for the TI-GER Board (not included) for microcontroller. The EVM is only a power board.

    -Nick