Is any documentation on Fast-Slow decay for the drv8432 .
Slow Decay:
Can be used in the following combination
Drive:
A= PWM, B=0
~A=0 ~B=PWM
Slow Decay :
A = 0 B=0
A=1 ~B=1,
~B will be =1 all the time , is any concern doing this for the drv8432.
2) Is any different way to use Fast Decay than Resetting AB and CD ?
3) I would like to know in which c file in the drv8412EVM REVG the decay is controlled to see hay is done at 4000 steps per second
Albert