I need to control the motor orientation using a digital output (LOW or HIGH) from an external protoboard (e.g. Arduino or IOIO). For that, I need to remove the J1 jumper and connect the output pin from the protoboard to the EVM FR pin. Is the FR pin the one with the red square around or the round one on the top?
https://lh4.googleusercontent.com/-NWgrknKq1Io/UlN1XlKP2jI/AAAAAAAAA54/Fdi_oQ-YZG0/w517-h432-no/FS.png
Thanks!
-Al