This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV11873EVM - Motor stops over 9500rpm

Guru 19775 points
Other Parts Discussed in Thread: DRV11873EVM, DRV11873

Hi Team,

Our customer is evaluating the device using the DRV11873EVM.

They want to use the device to control the motor at 10000rpm, but the motor always stops at around 9500rpm.

What is the problem ? Is there anything that limits motor speed ? LS pin setting ?

[Customer Condition]
- Motor type : Star wiring motor
- have no changes on the EVM
- They tried changing VCC or PWM frequency, but no change.
- Load current at 9500rpm is 100mA, 150mA(peak), not in current limit.

Best Regards,
Kawai