Hi,
I am using a DRV8811 to drive a stepper motor and am looking for some application assistance:
The application uses full step control to move the motor through a fixed number of steps. In the past once the motor reached its required position the H-bridge was de-activated using the enable function and the motor windings are therefore un-powered and is hence he motor free to move.
My requirements haveI now changed so that once the motor has transitioned the demanded steps the mechanism is held in this fixed position and will not move under externally applied load.
The data sheet implies that with the enablen pin tied low the H-Bridge is always active and hence a drive currnt should be present on the output but I am not seeing a drive current on either of motor windings.
Is tthis correct ? If so then is there a way to hold the motor in its fixed position ?
Regards
Fiona