Team,
Here're some questions from emails on the DRV8307. I'm translating since the original messages were in Chinese. I've also copied Distributor James Su from Yosun, and TSR Aaron Chen in bcc.
1. there's a delta-connected 3-phase BLDC motor, running at 9000RPM 12V/5A when driven with old MCU solution. when moving to DRV8307, the motor didn't move. is DRV8307 able to spin delta-connected motors (vs. Y-connected)?
2. Rising / falling edge of the below waveform on phase voltage seems to be too long - is this correct?