This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi everyone,
Could the gate driver of the DRV8301 get broken because of not having a resistor in series with the MOSFET gates? It seems to be the origin of my problems. My PCB has worked before with smaller MOSFETS without a gate resistor, but now with bigger ones has only worked once, and then dead. I am getting FAULT and GVDD_UV. GVDD remains at 2V.
Regards.
Daniel
Hi Daniel,
Can you provide more information?
Were the FETs damaged on the board also?
Can you provide a schematic and layout?
What is the PVDD voltage? Is it possible that PVDD saw a spike above the absolute maximum?
Also please take a look at the post ( LINK ), where another user described a similar problem. In this case, inductive spikes were created damaging the DRV8301. The method used to correct the problem was also stated.
Hi Rick, thanks for the quick response. The FETs have been replaced and nothing has changed. They are rated at 160A. They input voltage comes from a regulated power supply at 15V (quite below the maximum) and a current limit of 5A. Tha capacitor on GVDD is not the one in the schematic, but a 4.7 uF 100V ceramic one.
The schematic is here. I am not allowed to post the layout as is.
Very interesting post the one you linked before. However, I still have 2V on GVDD when powered on, and the SPI is throwing coherent values for Control and Status registers. So I dont think there is a PVDD issue.
Hi Daniel,
GVDD should be ~11V typical. If GVDD is reading 2V then something has gone wrong.
Can you post the PN of the MOSFET that gave no issues and the MOSFET that had issues. It would be good to examine the differences.
I would recommend changing the GVDD capacitor to the recommended 2.2uF just to rule that out.
I would also take an o-scope and examine the gate drive slew rates (GH, GL, SH). Most issues with the DRV8301 results from switching the external MOSFET to fast. You can slow down the slew rates by lowering the gate drive strength setting and adding series resistance.
At fast slew rates, parasistic inductance in the half-bridge will cause voltage spikes (both positive and negative). These can be quite extreme. This is improved with reduced slew rates and improving the layout around the half-bridges.
Daniel,
The slew rate current strength affects how fast the gate of the external MOSFET turns on. An extremely fast slew rate can cause voltage ringing on the external half-bridge due to parasitics in your layout and the MOSFETs themselves. This ringing can potentially damage the DRV8301 if it is severe enough (it cannot protect against this, it must be managed in system design).
The gate charge (Qg) of the "larger" MOSFET is actually 3x the smaller MOSFET, so you may actually be under driving the MOSFET. The best way to check this is to examine the gate drive voltages and see what is actually happening. I would do this first before making a change. We need to understand what is actually happening between the two MOSFETs
I would not install more than 1-30 ohms of resistance.