Hi,
I use a STM32F7 controller to feed in the PWM signals into INH & INL pins.
When the motor starts, the outputs(GH&GL) makes the right signals that corresponds to the input signals.
However, after a bit, the output starts to fall apart and I can't find a reason why this is happening.
Please advise.
As shown above, Pink is the input PWM signal and Yellow is the output PWM signal(towards the MOSFET's gate).
You can see that on the left of the waveform, the yellow follows pink pretty well, but it starts to fall apart.
Thanks,
SJ