This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8307: Motor drive issues

Part Number: DRV8307

Would someone mind reviewing the attached RevB schematic and gerbers for this updated Motor Driver Board?

My issue with this revision:  I need to drive the motor at 5000 RPM, but the driver board seems to be maxing out at around 2400 RPM.  I suspect it's hitting current limit, but not sure.  The motor is rated at 6000 RPM at 9 amps.  I have a .028 ohm current sense resistor.

5078.motor schematic.pdfMotor Driver Layout_all.pdf

Steve