Other Parts Discussed in Thread: DRV8703-Q1, DRV8702D-Q1, DRV8703D-Q1, DRV8702-Q1, DRV8305-Q1
Hi team,
The customer would like to select a motor drive device for the automotive application.
His requirements are as below:
1. The power supply should be 8V~16V.
2. The peak current is about 8A~10A.
3. The continuous current is about 5A.
4. The operating ambient temperature should be -40C~125C.
5. It is best to have the EVM board to help develop.
So, I recommend DRV8332-HT. But it does not have the EVM board.
Do we have other better motor device?
How about the Brushless DC Gate Drivers? Do we have the Brushless DC Gate Driver that can meet the customer's requirements?
If we have, would you recommend a MOSFET that can meet the customer's requirements?
Best Wishes,
Mickey Zhang
Asia Customer Support Center
Texas Instruments