Hi,
I have a BLDC motor with 3 linear hall-effect sensor. Is there any BLDC motor driver IC that has 3 linear hall-effect sensor input. or is there any decoder IC can decode these 3 linear hall-effect sensor signals. Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have a BLDC motor with 3 linear hall-effect sensor. Is there any BLDC motor driver IC that has 3 linear hall-effect sensor input. or is there any decoder IC can decode these 3 linear hall-effect sensor signals. Thanks.
Hi Rick,
Thanks for your reply. I saw the datasheet of DRV8307 and DRV8308 to find the input of hall sensor is POSITIVE and NEGATIVE for the hall sensor of every phase. But the linear hall sensor only has one pin to output a sine waveform. How can I connect one pin of the linear hall sensor to two pins of POSITIVE and NEGATIVE input of DRV8307 or DRV8308. Thanks.