This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8860EVM: Source code for slvc530a application

Part Number: DRV8860EVM
Other Parts Discussed in Thread: DRV8860,

Where can I download the source code for this application?  I'd like to copy/paste sections of it into our product application (an embedded system) so I don't have to re-invent the wheel for the basic communication/API to the part (since it's a unique serial protocol, etc.).  I've seen many blogs where people have had various difficulty in just getting a basic communication going with the part, and I want to avoid all that - so we can move on with ordering many,many DRV8860 units for our product.

Thank you very much!

Brad

  • Hi Brad,

    The source code can be found in the DRV8860EVM_MSP430_FIRMWARE.zip file in the Hardware files of the DRV8860EVM.

    The direct link is: http: //www.ti.com/lit/zip/slvc596

    Depending on the age of the EVM, the source code is either in the Hardware files (older) or Software files (newer).