This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8303: OCP triggered

Part Number: DRV8303

Hello, I use drv8303 with bldc motor and 3 shunts with 50A mosfet. OCP is triggered with 45A threshold. I see high currents during lowside mosfet commutation, mainly on one phase. WHen I modify motor phases connections, THe high currents occure on the New corresponding phase, as if it dépends on the motor inductance. I see high currents on the shunts and they propagate on GND and éven on Gate Mosfets . How can I reduce those short circuits during mosfet commutations?

Sincerely yours

Dominique Houzet