Hi Team,
My customer asked following questions about DRV8832-Q1 Datasheet.
(1)OCP time
In 7.3.6.1, datasheet says “If this analog current limit persist for longer than the OCP time, …” but it seems no description for OCP time. Could you provide OCP time?
(2) 8.2.2.2 Motor Current Trip Point
In this section, there is a description as below.
"To set IILIMIT to 0.5 A, RISENSE = 0.2 V / 0.9 A = 0.22 Ω."
For the part of "To set ILIMIT to 0.5A", is it typo and should be corrected to "To set ILIMIT to 0.9A"?
Best regards,
Nobuo Fujihara