Other Parts Discussed in Thread: DRV10983-Q1, DRV10974, DRV10964, DRV10975, DRV10963, DRV10975EVM
Greetings:
Would like to know if there is any DRV____ evaluation module with the (optimal) closed loop MCU controller included.
The DRV10866EVM has two PWM and FG pins to allow optimal closed loop MCU control.This is for a 5V system.
I need to build and test a DRV system with closed loop MCU control. The 3-phase BLDC motors are powered from an automotive battery (12V typ) .
I need to have accurate control and be able to program (ramp up/down, maintain constant) the BLDC RPM.
What would you recommend? Thank you.