Other Parts Discussed in Thread: DRV8323, DRV8307, DRV8306
Can I use the UC2625 to drive the DRV8323 Gate Driver in a 50V, 20A Brushless DC Motor Driver design ? if so, are they any special design instructions that I need to be aware of?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thanks Brian for the recommendations. My requirement is that I have to implement an analog control scheme the takes hall inputs , an analog motor current command, and generates the proper commutations. Moreover, I have to be able utilize a 50V source to drive the motors with out adding additional voltage regulators on the board due to other constraints.