This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8837C: chip is burned out

Part Number: DRV8837C

application: bike lock

2 chip is tested ,after 1000-times test,one is burned out.

vm=4.2V,  Iout<550mA

test is bellow: a single cycle

( in1,in2 =01

after 1s ,

in1,in2=11

50us delay,

in1,in2=00

50us delay,

sleep =0 )DRV8837C 烧芯片问题.zip

after burning out the chip, testing the resistence,

the resistence between the VM and GND =1.8 ohm

the resistence between the out1 and GND =1.4 ohm

the resistence between the out2 and GND =1.4 ohm