Other Parts Discussed in Thread: DRV8886, DRV8886EVM
Hi Support,
Can DRV8818 drive a unipolar stepper motor?
If can’t, could you help to propose a unipolar stepper motor driver, with the following requirements?:
Requirement
Power supply: 24V
Motor speed Requirement: 1500rpm (25 rev/sec, 40,000pps @ 1/8 microstepping)
Motor Acceleration: High
Microstepping operation requirement: 1/8
Load: 12kg
Unipolar Motor Specs
Rated Voltage (V/phase): 3.6V
Rated Current (A/phase): 2.0A
Winding Resistance (ohm/phase): 1.8 ohm
Inductance (mH/phase): 2.5mH
Thanks.