Other Parts Discussed in Thread: DRV10983
Hi Team,
I'd like to use the DRV8332-HT for its guaranteed 1000hours over 165°C, the drawback I face now is that I should control it with 6PWMs or 3PWMs which is complicated; I need a more simple controlled device with one PWM like happened in the DRV10983.
1• Suggest please another chip with same specs but one PWM signal controlled like the TI sensor-less BLDC motor control drive in: DRV10983
(even if obliged to add external DMOS circuit)
Or
2• Could you support how to use or add another high temp TI IC controlling DRV8332-HT through its 6PWMs signals
Regards