This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
After the motor rotation stops, there is noise inside the motor. The motor is locked. And there is no PWM wave input on the measurement step. When the motor is directly stopped at the start, the motor is locked without noise. The motor drive configuration has been changed all over again. The customer wants to know why there is noise?
Thanks.
Hi Annie,
I have a couple questions:
Hi Pablo Armet,
I have sent the private message to you. Would you help to check it?
Thanks.
Annie
Hi Annie,
I have received your private message and I am currently reviewing it.
In the meantime, can you kindly confirm if what I am saying below is true (please correct me if my assumptions are incorrect) :
Thank you!
Hi Pablo,
The motor will stalled at different frequencies. The motor is not stalled at 6khz and 10khz. However, when it is lower than 10khz, the stall will occur and the motor will still rotate. It is not a fault alarm, and the motor will heat up after a long time of stopping. He used 2.8A motor. According to the manual calculation, the current is 1.7A.
Thanks.
Annie
Hi Annie,
[Q]: Can the customer provide a picture of their set-up?
[Q]: Can the customer provide a screenshot of the output PWM signals and FAULTn when the motor is stopped with frequency below 10kHz and above 10kHz?
[Q]: can the customer provide a scope shot of the PWM signals of at least two outputs when the audible noise is heard from the motor? It could be that the motor is holding current which can lead to some audible noise.
Hi Annie,
I have not heard back from you. I am assuming you're issue has been resolved. If not, please post a reply below. If thread is locked, click on "Ask a related question" button to post a new question