Hi
I am going to control the speed of a BLDC motor from 0 to 60 RPM/min.
There is no hall sensors on the motor, but if needed it might be possible.
There is practically no load on the motor, only a small plactic container.
It should be possible to adjust the speed in 0.2 RPM/min steps e.g. 10.2 RPM/min or 10.4 RPM/min
It must also be possible to reverse the direction when running at e.g. 10 RPM/min. The motor should decrease to zero and continue up to the reverse speed with no interruption.
Can this be done with the DRV10974?