Hello,
I am using the DRV8832-Q1 as a Dual H Bridge, and I am trying to disable the PWM getting 100% Duty Cycle.
My settings are as follow:
VCC 4V
ISENSE=GND
OUT1 - OUT2 Via 100Ohm for testing
IN2= 0
IN1 = 3ms pulses every 500ms
VREF -VSET Via 5k
VSET - GND Via 180K
FAULTn - Not Connected
When the IN1 Pulse is 25ms I get the PWM
When the IN1 Pulse is 3ms, the Drain (N Ch Fet) doesn't even start.
I would like to know what is the minimum pulse time I need to use and how to get the 100% DC
I have also tried to connect VREF to VSET directly and I get the same result.
Please advice