Other Parts Discussed in Thread: DRV10987, DRV8320
Dear experts,
This might look like a stupid question but please give your time to help me asap.
I have a BLDC motor (24V - 100W) called nema23 with specs as below picture:
1/ Can DRV8308 work with this specific motor?
2/ If possible, please provide the detailed connections according to this motor (especially for Hall connection)
3/ I will use a microcontroller to control speed, pwm mode, direction and brake. What can I do to make this motor run. I mean the detail step by step such as setting up mandatory parameters, and through spi or what?
I have read through the datasheet of DRV8308 but could not conclude all needed steps to make the motor run. I need to finish my prototype asap then will run into mass production.
Thanks in advance,
Dientu28