This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV10970EVM: Issues controlling a motor with this EVM

Part Number: DRV10970EVM
Other Parts Discussed in Thread: DRV10970,

Hi Everyone,

Initially, I was able to get the DRV10970 EVM to spin a brushless motor. Unfortunately, it no longer drives the motor and no longer illuminates the locked rotor LED. 

I'm using a small brushless motor with 3 Hall IC's. I soldered 2.2kohm resistors on R17-R19 as pull-up resistors and placed jumpers on J5, J7, and J8.

I can see that the PWM is working from the potentiometer/555 timer, but the UVW phase outputs are measuring ~70mV regardless of the potentiometer position. Other voltages such as VINT and HPWR are correct. I've tried a few different motors and I've also tried every combination of hall/phase wiring to rule that out. 

Is the PCB broken? Any info or tips are greatly appreciated.

Thanks,

Tim