Other Parts Discussed in Thread: DRV10974, DRV10964
Hi team,
We use DRV11873 with 6 pole pair.
We hope to drive 10800rpm but this device can't achieve this operation according to the https://e2e.ti.com/support/motor-drivers/f/38/p/314799/1096171#1096171, is that correct?
Because RPM=(FG*60)/pole pairs=(950*60)/6=9500rpm.
If 10800rpm can't be achieved, do you have an alternative device which is pin and function compatible?
When I searched TI.com, DRV10974 is same package but not same pin assignment.
Best regards,
Koyo