According to the section 2.4: "Modulate the PWM input between 2 duty cycles 1% to 2% apart. Do this every 1 to 1.5 seconds to prevent the FG frequency matching the internal sampling frequency. The result is an average speed of the two PWM duty cycles." in the documentation "DRV11873 Lock Detection Functionality".
I changed the PWM duty cycles 1% to 2% every 1 to 1.5 seconds, and tried it all the different combinations, however, I still have the lock dection problem. The motor restarts irregularly when the FG frequency falling into the range from about 466Hz to 486Hz.
Does someone have any suggestion to solve the problem? Thank you so much!