Hi Team,
The customer is experiencing below issue and needs your help.
1. VM has been connected to the 5V power supply generated by external step-down, but the gate drive voltage is still equal to the bus voltage? This problem also occurs on the evaluation board of drv8353rs-evm. The customer did not change any configuration of the evaluation board. R19 resistance is welded, but the gate drive voltage is still equal to the bus voltage
2. Whether the delay from 8353 input to output of the PWM used for control has measured data?
3. Does the gate drive between output of drv8353 and the MOS gate do not require any other auxiliary circuits such as gate resistors?
4. Can the internal integrated op amp of drv8353 not be connected to the input? If it is not connected, can it be suspended, can it be suspended by using only two of the channels? If it can not be suspended, how to deal with it? Are the control cores in the op amp and drv8353 independent of each other? Will the control core not work if the op amp does not work? Does the op amp support differential input?
Thanks,
Annie