Part Number: DRV8432
Hello,
Would it be possible to set the overcurrent threshold by feeding a reference voltage into the OC_ADJ pin, rather than using a resistor? This would allow a dynamic current limit, so it could be set to minimum at start-up, and then increased when certain criteria is met for example. Also, is 1.4A per bridge (plus tolerance) the absolute lowest limit that can be set?
Many thanks,
Stephen