Hi, team.
The data sheet has the following description, is 800 ns typo?
"The voltages applied to the inputs should have at least 800 ns of pulse width to ensure detection. Typical devices require at least 400 ns. If the PWM frequency is 200 kHz, the usable duty cycle range is 16% to 84%."
What is the minimum pulse width?