We are looking to design a 3-phase DC motor controller for an electric scooter.
The motor is a brushless DC motor, with three hall sensors, 72vdc, 40A, 3-phase motor.
The target processor is the TMS320F280x series of Piccolo™ Microcontrollers using the InstaSPIN-FOC firmware.
Our inputs are one analog 0-5vdc from the throttle, the three hall sensors, two digital inputs from the brakes, battery monitor which includes battery capacity and communications to a user interface.
Can you identify a processor that will work with our 72vdc, 40A requirement the highest voltage part I can find is 42vdc using 60v MOSFETs or a way we can signal condition to use one of the existing processors?
We also want regenerative braking, does the TMS320F28xx series have the firmware to perform this function?
Any information would be appreciated, possibly there is a reference design we can start with and modify for our application.
Thank