This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV110: EN pin maximum voltage

Part Number: DRV110

Hi,

What is the maximum voltage we can apply on the EN pin of the DRV110?

I blew one IC after using 24VDC to toggle ON/OFF. Then I used the evaluation board DRV110EVM and measured 5 Votls on the EN pin.

I could go with 5 Volts but I would like to know the limitation of this input.

thank you.