Other Parts Discussed in Thread: DRV8812, DRV8824
Please tell me the mechanism.
What percentage is acceptable from 0.01uF?ask.xlsx
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Let me research this and I will get back to you by Nov. 18 (United States time).
Hello,
I tried to replicate your results in the lab but was unsuccessful. The motor was running normally even with a 0.03uF bypass capacitorv (/cfs-file/__key/communityserver-discussions-components-files/38/bypass_5F00_cap.pdf). I believe the reason for difference results could be from having different motor and set-up/equipment.
I want to confirm whether the behavior you are seeing is due to the bypass capacitor value or if it's due to a test setup or layout issue.
Could you kindly provide me with the following information:
Hello
About the board layout and the motor information please reference the insert file
I tried the 1KHz and 14.5KHz (STEP) however, the motor was running normally
Did the capacitor value relate to STEP?
Could you kindly tell me why the recommended VM capacitance value is 0.01uF (mechanism)
If increase that value, motor will be running abnormally?
Thank you!bypass.xlsx
Hello,
Thank you for providing the information.
I looked at your set up and the information on the file. I have a couple things I want to point out:
I suggest trying the following:
[Q]: Could you kindly tell me why the recommended VM capacitance value is 0.01uF (mechanism). If increase that value, motor will be running abnormally?
[A]: The Vm capacitance value is recommended from the design team. They run multiple simulations to find the value which will work best. In your case, increasing the value from 0.01uF to 0.03uF should not cause the motor to run abnormally.
Hello,
I am glad to hear the motor is running normally. I have the answer to your questions below:
Hello,
Please take a look at this thread (e2e.ti.com/.../1908513. This thread explains the reason for the 1Mohm resistor. The post is for the DRV8824 but the concept still applies to the DRV8812.
In short summary, adding the resistor is optional to the DRV8812. There will be no change to the device's performance or design functionality if the resistor is not added. Likewise, the resistor is also optional for the DRV8885 for the same reason.