Hi Team,
I would like to seek assistance for our customer product request.
Here is the requirement for BLDC motor driver with PID control option (IC and EVM):
- Control 10 ~ 25W class motor using Hall sensor.
- Motor driver Vcc: 5V or above
- Motor Voltage, current : 12 or 24V, 2.3A_Max
This is to control the shaking caused by the slight speed difference that occurs at the constant speed of the motor.
I read this document below regarding "Sensored 3-Phase BLDC Motor Control Using MSP430" but there's no BLDC motor driver IC product mentioned:
http://www.ti.com/lit/an/slaa503/slaa503.pdf
The nearest I found is TIDA-01585 but is a PI control so I hope you can recommend a more fit to customer request.
Thanks!
Jonathan