Can the DRV8870 be used to operate as a high side driver or as a low side driver?
Example 1: Can the OUT1 pin be utilized as a high side driver output when connected to drive one side of a solenoid with the other side of the solenoid connected to circuit ground? The device H-bridge control pins would be configured such that only one control pin, IN1, would be used to drive current out the OUT1 pin. We would not have the option of using both the OUT1 and OUT2 pins directly as one side of the solenoid would already be referenced to circuit ground and it cannot be moved/connected to the OUT2 pin.
Example 2: Can the OUT2 pin be utilized as a low side driver output connected to drive a lamp with the other side of the lamp already connected to the same supply voltage as the VM pin? The device H-bridge control pins would be configured such that only one control pin, IN1, would be used to drive current into the OUT2 pin. We would not have the option of using both the OUT1 and OUT2 pins directly as one side of the lamp would already be connected to the supply voltage and it cannot be moved/connected to the OUT1 pin.
Given both examples, can the ISEN (current regulation) function still be utilized for either or both configurations? Maybe only the low side drive configuration?
The data sheet Functional Block Diagram indicates that Over Current Protection (OCP) is provided on both the high and low side outputs, OUT1 & OUT2. If the device can be utilized as a high side or low side driver will the OCP feature still work in both configurations?
Thank you for your help.