Hello,
This question is relevant to my post "DRV8889-Q1: Device Behavior".
I'm still wondering how to detect an open-load condition correctly with DRV8889-Q1 even at an electrical angle of 0°, 90°, 180°, or 270°. I thought one way was to monitor OL_A or OL_B bit of DIAG Status 2 register. If I knew the current electrical angle of the DRV8889-Q1, I could mask the status of OL_A or OL_B by MCU when the angle was at 0°, 90°, 180°, or 270°.
How can I know about the current electrical angle of DRV8889-Q1?
Best regards,
Shinichi Yokota