I am having troubles making the DRV2700RGPT work.
After successfully using the DRV2700EVM for my application, I have designed my own PCB and let a professional PCB manufacturer assemble it. I have used the layout from the DRV2700 Datasheet (Figure 22, values of components below).
EN has been fixedly programmed at “1”, Gain = 38.4 dB, V_PVDD = 105V.
First, I connect the piezo. Then I connect the input signal (differential, from a AC signal generator). Then I connect the power. In this sequence. I believe I have already damaged 3 PCBs.
In the first trial, I managed to measure V_FB = 1.15 V and V_BST = 105 V. The quiescent current from the power supply was 72 mA when input signal was muted, and around 230 mA, when input signal was maximum. I managed to make this work for a few minutes. But when I connected a different piezo to the output, the quiescent supply current surged to 500 mA (limited by my power supply) and no output was generated. Since then, I was not able to make this circuit work again and the 500 mA is always there, so I disconnect it quickly.
Can you please tell me what is the problem with my design?
I have read the DRV2700EVM datasheet as well, and all the E2E Forum replies, but I can’t find the right answer.
Please let me know.