Other Parts Discussed in Thread: DRV8312, , TMS320F28034, TMS320F28035
Rise/fall time: DRV8313 150nsec → DRV8312 14nsec
Propagation delay time (from inputting PWM signal to IN until actually outputting signal from OUT)
tpd on 500nsec max → DRV8312 38nsec
tpd off 475nsec max → DRV8312 38nsec
Dead time
DRV8313 90nsec → DRV8312 6nsec
DRV8313 is about 10 times slower than the above.
Compared with the DRV8313 and DRV8312, is there a difference in the timing when UVW three-phase drive is performed after the PWM output from the control microcomputer is input?
Is there any deviation in the timing of sampling the phase current?