Hi, I have two questions on nFault pin of DRV8343-Q1.
1) In DRV8343X-Q1EVM, the nFault pin is connected to 3.3V LDO with a pull-up resistor R51. I am wondering whether I can leave the pin open. If not, could I connect the nFault pin with a 5-V source from a DC-DC converter because my design doesn't have a 3.3V LDO but have a 5-V from a DC/DC converter that is used to source a MCU.
2) If DRV8343S-Q1 is used, the nFault pin is an active-low fault flag which will be low when a fault is present. My customer requests to Fault output be an active-high fault flag, which will be high with a voltage of VBB (12-V or 24V based on the battery) when a fault is present. Could you please advise how to use an external circuit to make it happen?
Thanks,
John