Hi team,
My customer is evaluating the DRV8662EVM. Could you please support the following questions?
1) A 2 V offset voltage is observed at the input after the coupling capacitor (C4, C5). Therefore, if JP2, JP3 is removed, in+ and in- are fixed at 2V respectively. So is there an internal circuit that offsets the input of the DRV8662?
2) I think there is a statement in the data sheet that a coupling capacitor should be inserted for IN + and IN-. The evaluation board also follows the instructions. I want to drive a piezo actuator with a 50Hz square wave. Is it okay to remove the above coupling capacitor? Or, I would appreciate it if you could tell me the know-how for driving the above.
Regards,
Yamaguchi