Hello,
I am working with the DRV2605L Haptic driver and I’m driving an ERM. We are planning on using some of the library waveforms for our haptic indications.
I was looking through the data sheet specifications about diagnostics for a document I am writing.
We will be playing waveforms using MODE=0x00 (REG0x01 [2:0] = 0x00), Internal trigger.
I see there is an option to put the chip in Diagnostic mode by setting the MODE to 0x6 (REG0x01 [2:0] = 0x06)
If we set MODE=0x06(Diagnostics) does this run the motor when the GO bit is set?
If Diagnostics are performed for the MODE=0x00 and for the MODE=0x06 do they both test the conditions for DIAG_RESULT,FB_STS,OVER_TEMP and OC_DETECT bits?
How long the Diagnostics test last or does it depend on the ERM?
Thanks,
Adam