Other Parts Discussed in Thread: TPS65218D0, TPS65218
HI TI!
We have a PCB design with the TPS65218D0. For a new production can we replace the TPS65218D0 with the TPS6521845? (Without making changes to the PCB or BoM).
Maybe I just have to reprogram the chip via I2C, but it should not be a problem.
My doubt is because on page 2 of the TPS6521845 datasheet they put the inductor of L1 and L2 with value of 1.5uH (same as TPS65218D0/15/25, ) and L5 with value of 10 uH (different from TPS65218D0/15/25).
However on page 20 of the TPS6521845 datasheet they put the inductor of L1 and L2 with value of 10uH (different from TPS65218D0/15/25, ) and L5 with value of 10 uH (same as TPS65218D0/15/25).
Please see the attached picture.
Also on page 20 of the TPS6521845 dataseet the pull up voltage levels for pgood and nWakeUp are swapped with respect to the TPS65218D0/15/25 dataseet. Please check the attached image.
I think these are datasheet editing errors and the chip can be replaced without problems. But we prefer to confirm with TI.
Thank you very much.
Best regards